PCA Bar Charts

To access the PCA Bar Charts, click the View Bar Charts button on the PCA model view.

Bar Chart options

Choose between the following bar graphs:

  • Loading plots of principal components: These bar charts show the loading of the input variables on the principal components.

  • Scree plot: The bar chart shows the contribution to proportional variance the principal components have on the scree plot.

Customize the display:

  • Show labels: Toggle the visibility of the bar labels.

  • Show values: Toggle the visibility of the bar values.

  • Sorted by value: Toggle the sorting of bars according to value in descending order.

  • Auto scale visible: this check box is used to scale the bin heights in the bar chart.This is only available when comparison data is loaded.

    • If selected, then the maximum height of the Y-axis will be that of the maximum bin height in the current view.

    • If de-selected, then the maximum height of the Y-axis will be that of the maximum bin height of the entire dataset.

 


Related topics:

  

CSense 2023- Last updated: June 24,2025